AXIS#.VL.ARTYPE1 to AXIS#.VL.ARTYPE4

Description

These parameters indicate the method used to calculate the biquad coefficients AXIS#.VL.ARPFx, AXIS#.VL.ARPQx, AXIS#.VL.ARZFx, and AXIS#.VL.ARZQx. A value of 0 indicates that the coefficients are set directly. This parameter has no effect on the filter itself, but is only used to determine the original design parameters.

Value Definition
0 Unity: Biquad is in a pass-through state, unity at all frequencies
1 Lowpass: Standard two-pole lowpass filter
2

Notch/Resonator: A standard Notch filter with selectable bandwidth, frequency and depth - can also be used to create a positive notch(Resonator) by making the gain positive

3

Lead/Lag: Filter with unity gain at low frequencies and either high gain (Lead) or low gain (Lag) at high frequencies, with the center frequency and gain user selectable

4

Biquad: Biquad is opened up with raw values on the numerator and denominator for the user to customize.

5

Auto-tuned Biquad: This means the filter was tuned by the Autotuner - manually changing this filter cannot guarantee stability.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

AXIS#.VLARTYPE1 = 1

AXIS#.VLARTYPE2 = 4

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.ARTYPE1

5011h

0ch

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE2

5011h

0dh

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE3

5011h

0eh

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE4

5011h

0fh

Signed8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6008

1

6008 (0x1778)

AXIS1.VL.ARTYPE1

Signed8

Read/Write

Yes

71544

2

6008 (0x1778)

AXIS2.VL.ARTYPE1

Signed8

Read/Write

Yes

6009

1

6009 (0x1779)

AXIS1.VL.ARTYPE2

Signed8

Read/Write

Yes

71545

2

6009 (0x1779)

AXIS2.VL.ARTYPE2

Signed8

Read/Write

Yes

6010

1

6010 (0x177a)

AXIS1.VL.ARTYPE3

Signed8

Read/Write

Yes

71546

2

6010 (0x177a)

AXIS2.VL.ARTYPE3

Signed8

Read/Write

Yes

6011

1

6011 (0x177b)

AXIS1.VL.ARTYPE4

Signed8

Read/Write

Yes

71547

2

6011 (0x177b)

AXIS2.VL.ARTYPE4

Signed8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.ARTYPE1

6008

Signed8

Read/Write

-

AXIS1.VL.ARTYPE2

6009

Signed8

Read/Write

-

AXIS1.VL.ARTYPE3

6010

Signed8

Read/Write

-

AXIS1.VL.ARTYPE4

6011

Signed8

Read/Write

-